{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is maximum sound/noise level of the MV transformer?
Maximum sound power level for MV transformer would be compliant with Energy Networks Association ENA TS 35-1 requirements. Please see attached Schneider transformer data including sound levels.
Sound level tests on transformers for more specific sound level data, are not a routine test requirement – they are a “special” test as defined within IEC60076, as such not carried out unless specifically requested when order is placed.

Lower transformer sound power levels are also available should they be required – achieved by bespoke/ETO specific designs.

Schneider Electric Ireland

Attachment(s)
998-21295210_Transformers_Ecodesign_Tier2_GMA_Brochure.pdf [8.97 MB]