{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Trip temperature of the braking resistance

If you are talking about the contact of the braking unit (highlighted in orange) then there is no value to communicate because it is not jut a thermal contact with a threshold. It is a calculation of the thermal state of the IGBT inside the unit that takes into account several parameters, temperature measurement the cooling air...

From manual

If you are talking about the thermal contact braking resistor associated to the braking unit (highlighted in green) then the threshold depends on the resistor used. Generally in our resistor it is around 120c°.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: