{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

MTZ Maximum Zs figures for 0.4 seconds disconnection

The Zs for MTZ used to be done from the settings on the Micrologic X and using the following formula - Zs = 218.5/In x Ir x Isd x 1.1

Where - 218.5 is the 230 voltage to earth multiplied by the Cmin factor 0.95 divided by - In = Device rating x Ir = Long time dial setting x Isd short time setting x by 1.1 a 10% tolerance for the Isd short time setting.

Now it can be done easily by entering your figures into the attached (Related Tab) Excel file.
A 1000A example has been entered on Line 5.

Schneider Electric Ireland

Attachment(s)

MTZ Zs 0.4s file.xlsxMTZ Zs 0.4s file.xlsx [11.57 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: