These devices are not deemed a true S type and so that the figure may be different to the S Type time delayed operating time of within 130-500ms .
For our Vigi MH type the break time should be 300-800ms when the intentional delay is set to 310ms.
The break time declared by SE is based on the request of IEC60947-2 annex B.
Please see the attached extract in the related tab.
Released for:Schneider Electric Ireland