{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
which is the alternative for HMISTU655?

If you are using the HMISTU655 then you can easily replace the HMI with any of the following HMIs inside the Harmony HMISTU range:

  • HMISTU655W : Same characteristics as HMISTU655 but there is not any Schneider Electric logo on the front part.
  • HMISTU855 : Same rear part but bigger screen (5.7").
  • HMISTU855W : Same rear part but bigger screen (5.7") but there is not any Schneider Electric logo on the front part.
  • HMIS5T + HMIS65 : These are the two (2) parts of the HMISTU655 (rear + front).
  • HMIS5T + HMIS65W : These are the two (2) parts of the HMISTU655W (rear + front).
  • HMIS5T + HMIS85 : These are the two (2) parts of the HMISTU855 (rear + front).
  • HMIS5T + HMIS85W : These are the two (2) parts of the HMISTU855W (rear + front).

If you are using the HMISTU range there is a chance that you are using the Vijeo Designer Limited Edition so if you need another HMI different than the HMISTU range then a license for Vijeo Designer is needed.

If you have a license of Vijeo Designer then you can use any of the following HMI from the Harmony GTO.

  • HMIGTO1300 : This HMI does not have the 22 diameter hole to install the HMI on the enclosure and the size of the screen is 3.5" , no ethernet communication.
  • HMIGTO1310 : This HMI does not have the 22 diameter hole to install the HMI on the enclosure and the size of the screen is 3.5" , ethernet communication.
  • HMIGTO2300 : This HMI does not have the 22 diameter hole to install the HMI on the enclosure and the size of the screen is 5.7" , no ethernet communication.
  • HMIGTO2310 : This HMI does not have the 22 diameter hole to install the HMI on the enclosure and the size of the screen is 5.7" , ethernet communication.

It is possible that some manual adjustments are needed due to the different communication port between the HMIGTO and the HMISTU range.

Again, if you have a license for Vijeo designer then you can also use the Harmony GTU range but the minimum size is 7":

  • HMIG2U + HMIDT351
  • HMIG3U + HMIDT351
  • HMIG5U2 + HMIDT351

Another solution could be the HMISTO7 but the software is not Vijeo Designer, there is an internal tool to migrate the application but there is not any guarantee that the project will be migrate 100%.

For further information about the HMISTO7 please check the next FAQ:

https://www.se.com/uk/en/faqs/FAQ000229667/

Schneider Electric Ireland

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: