Search FAQs
Do we offer a replacement door cover for MG6P6?
MG6FCC6 is the closest replacement front cover we offer for MG6P6.
Be aware that it is all of the steelwork for an MG6 way 630A panelboard and not just the front cover. It is painted RAL9001 (cream/white) which differs from the original board (beige).
Finally the customer will have to locally adapt the front cover if they have fitted any of the following
Be aware that it is all of the steelwork for an MG6 way 630A panelboard and not just the front cover. It is painted RAL9001 (cream/white) which differs from the original board (beige).
Finally the customer will have to locally adapt the front cover if they have fitted any of the following
- Larger outgoing MCCBs (400a-630A Frame)
- CTs & Vigi blocks.
Released for:Schneider Electric Ireland
Explore more
Product:
Range:
Explore more
Product:
Range: