{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the equivalence of the XPSAL** and XPSAC safety module references**?

Article available in these languages: Spanish

The former XPSAL●●●●● safety modules were replaced by the XPSAC●●●●●.
The XPSAC** have been replaced by the new XPSBAC safety modules**
They have the following differences:
The XPS-AC includes a third safety contact.
The XPS-AC includes a static signaling output
The XPS-AC has a version with removable terminal block.

Depending on the supply voltage the replacement references of the old XPSAL and XPSAC safety modules are:
Supply voltageOld ReferenceCurrent Reference *New reference:
24 Vac dcXPSAL5110XPSAC5121XPSBAC14AC / XPSBAC14AP
48 V acXPSAC1321XPSBAC34AC / XPSBAC34AP
120 V acXPSAL3410XPSAC3421XPSBAC34AC / XPSBAC34AP
230 V acXPSAL3710XPSAC3721XPSBAC34AC / XPSBAC34AP
* Models with removable terminal block add a P to the reference.


Substitution Schemes Between XPSAL and XPSAC Safety Modules:
Monitoring an Emergency Stop with 2 NC Contacts

XPS-AL XPS AL XPSAL XPS-AC XPSAC módulo de seguridad Safety Sustituto,Alternativa,Sustituta,Equivalencia,Equivalente,Substituição

Monitoring an Emergency Stop with 1 NC Contact

XPS-AL XPS AL XPSAL XPS-AC XPSAC módulo de seguridad Safety Sustituto,Alternativa,Sustituta,Equivalencia,Equivalente,Substituição



Schneider Electric Ireland

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
move-arrow-top