Search FAQs
What is the contact resistance of a ComPacT NSX NA Switch-Disconnector?
For the contact resistance / resistance per pole for the ComPacT NSX NA switch-disconnector please see table below the micrologic trip unit table are the same values for the NSX switch disconnectors.
![Image_2023-12-05_08-21-14.png resistance per pole table](https://se.file.force.com/sfc/servlet.shepherd/version/download/0688V00000gIeFr?asPdf=false&operationContext=CHATTER)
This can be found in the catalogue link below from page 179.
ComPacT NSX & NSXm Circuit Breakers and Switch Disconnectors from 16 to 630A up to 690V - 2022 | Schneider Electric (se.com)
This can be found in the catalogue link below from page 179.
ComPacT NSX & NSXm Circuit Breakers and Switch Disconnectors from 16 to 630A up to 690V - 2022 | Schneider Electric (se.com)
Released for:Schneider Electric Ireland
Explore more
Product:
Range:
Explore more
Product:
Range: