{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Would it be possible to install a TNS SPD on a TN-C-S network?

Please note that the SPDs with the A9L prefix, which are compatible with TT and TNS, are also compatible with TNS part of TN-C-S networks.

In a TN-C-S network, the neutral conductor N and the protective conductor PE are combined (PEN) up to a certain point, then separated (separation of the neutral conductor N and the protective conductor PE). The A9L SPDs for TNS are therefore compatible with this type of network on the TNS part of the TN-C-S network.

For the TNC part of the TN-C-S network, a 3P surge protector compatible with TNC is required.

TNCS network

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: