שאלות נפוצות
InRow Firmware Upgrade via multiple NMC Cards(ACRC, ACRP , ACSC, ACRD)
Issue:
InRow Gen1 Firmware Upgrade via multiple NMC Cards(ACRC, ACRP , ACSC, ACRD)
Product line:
InRow Cooling
Environment:
Data Center Cooling
Cause:
Resolution:
See the attached document, which will explain how to install and execute an NMC firmware upgrade for multiple units that are using the same firmware. For example, if you have 102 ACRC101, or a total of 50 ACRP100s and ACRD500s. See list of units below that use the same firmware.
ACRC
ACRC100, ACRC101, ACRC103
ACSC
ACSC100, ACSC101
ACRD
ACRD100, ACRD101, ACRD200, ACRD201
ACRP (600mm units)
ACRP100, ACRP101, ACRP102, ACRP500, ACRP501, ACRP502, ACRC500, ACRC501, ACRC502, ACRD500, ACRD501, ACRD502
פורסם עבור:שניידר אלקטריק ישראל
קבצים מצורפים
גלה עוד
טווח:
גלה עוד
טווח: