Issue
I need to install or replace a module in my Symmetra Power Array UPS system. How do I do this?
Product Line
Symmetra Power Array
Environment
All serial ranges
Cause
Symmetra UPS are designed with modularity so that modules can be added or replaced as needed. This document contains a video to aid the user in performing the installation of a new module or replacement of an existing module.
Resolution
The following videos detail the process of replacing the Battery and Power Modules in the Symmetra Power Array UPS.
Symmetra Power Array Power Module Replacement
Symmetra Intelligence Module Replacement