המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is there a NetShelter Accessory Compatibility Chart that shows which NetShelter accessories, UPS, PDU, Symmetra, NetBotz, Air or KVM fit into a specific cabinet?
Issue:
A comprehensive accessory chart would make it very easy to identify compatible NetShelter cabinets and accessories.

Product Line:
NetShelter

Environment:
All versions and serial ranges.

Cause:
There is a need know which accessories, or other APC/SE products are compatible with a specific NetShelter cabinet.

Resolution:
Please see the attached document for a list of NetShelter accessories sorted by product family, and the cabinets they're compatible with.
All current NetShelter cabinets are listed horizontally across the top of the document. The accessories & products that install into the cabinets are listed vertically.
All skus have hotlinks to the APC website, and items that have special requirements have notes, or hotlinks to FAQs.
This compatibility chart also includes other APC/SE product families that can mount into a NetShelter cabinet, such as Smart-UPS, rPDUs, NetBotz, Rack Air and KVMs.

שניידר אלקטריק ישראל

קבצים מצורפים
v79 NetShelter Compat Chart by Prod Family with PDU UPS NetBotz Air_web.xlsx [1.21 MB]
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
什么是EcoStruxure架构与平台?
EcoStruxure平台是我们基于物联网的系统架构的核心,是施耐德电气构建和交付解决方案的技术基础。帮助企业从生产线连接到云端实现万物互联收集传感器到云的关键数据,加以分析,从而发现有意义的洞见。
使您能够基于实时信息和业务逻辑采取行动。我们的Ecostruxure平台提供了实现智能运营的互联互通性和互操作性的核心能力,以及上云的数字化服务的的基础设施。