שאלות נפוצות
What's the difference between ATS22..S6U and ATS22...S6 Softstart models?
Issue:
Differences between an ATS22..S6U and ATS22..S6 soft start models.
Product Line:
Altistart 22 ATS22
Environment:
All models, All series
Cause:
Altistart has difference voltage suffix S6U and S6.
Resolution:
The ATS22..S6 model requires 220vac control power and has 24vdc logic inputs.
The ATS22..S6U model requires 110vac control power and has 110vac logic inputs.
פורסם עבור:שניידר אלקטריק ישראל
גלה עוד
טווח:
גלה עוד
טווח: