Basic principle
For Sepam series 20 and series 40,
The saving of alarm message histories can only be done by a remote monitoring and control system since this is the only effective means of saving in a substation that includes several Sepam devices. The devices are connected in a Modbus network to the remote monitoring and control system.
However, there is a simple but effective way to save individual Sepam histories, if the customer accepts to connect locally to the Sepam with a PC.
The procedure is described below:
Sepam series 20
The only possibility consists of saving a screen copy as follows:
- SFT2841 is connected to the Sepam
- select the diagnosis icon, history tab
- save the screen by pressing ALT + Print Screen
- paste in a Word filing by pressing CTRL+V
- name and save the file
Legacy KB System (APS) Data: RESL166597 V2.0, Originally authored by LaVI on 06/20/2008, Last Edited by DaMi on 06/20/2008
Related ranges: Sepam series 20
פורסם עבור:שניידר אלקטריק ישראל