YES. The Communication Accessory ACE 850 is compatible with the Sepam 80 if the Sepam 80 Base Version is greater than or equal to V6.01 and if TCP/IP option reference 59754 has been placed the order.
Note: The cable between Sepam 80 and its ACE 850 (CCA614 reference 59751) must be plugged in on the Sepam 80 F Port.
פורסם עבור: שניידר אלקטריק ישראל