Issue
Page 13 of the catalog 48332-EN_Ver5.0 (filename: en5.0_48332.pdf) lists TCSESM163F23F0 as having 14 copper and 2 fiber ports and the TCSESM163F2CU0 as having 16 copper only for Connexium Managed switches. This is incorrect, the descriptions are reversed. TCSESM163F2CU0 should be 14 x 10/100BASE-TX ports and 2 x Fiber ports and TCSESM163F23F0 should be 16 copper only .
This page shows the incorrect switch Descriptions and Reference numbers (highlighted).
Product Line
Connexium
TCSESM163F23F0
TCSESM163F2CU
Environment
Resolution
This page shows the correct Description and Reference numbers.
Legacy KB System (APS) Data: RESL190814 V1.0, Originally authored by DaDz on 01/25/2008, Last Edited by DaDz on 01/25/2008
Related ranges: ConneXview, ConneXium - Ethernet
פורסם עבור:שניידר אלקטריק ישראל