שאלות נפוצות
Can an XBTL1000 application be converted to Vijeo Designer?
Yes. The Switch2VijeoDesigner Conversion Team offer services that makes it even easier to migrate XBTL 1000 applications created on terminals XBT F to Vijeo Designer applications for use on terminals XBT GT/GK and HMIGTO. Please contact Customer Service (888 266-8705) for a Quote.
The service provides:
.. analysis of the complexity of migration regarding: hardware, software, communication with PLCs, etc.
.. analysis of the new functional requirements
.. proposal for migration methodology
The possible deliverables include:
.. simple conversion
.. full migration of complex machines
.. migration to SCADA system
.. standardisation process for multiple machines
For more information on this service offer, please consult your US Regional Sales Office.