Issue:
A user require the information on ION6200's and ION7300's nominal current.
Product Line:
ION6200 and ION7300 series meters.
Environment:
ION6200 and ION7300 current inputs.
Cause:
A user require the information on ION6200's and ION7300's nominal current.
Resolution:
The nominal current of both ION6200 and ION73xx are both 5A. The installation guides of these meters only list their rated current at 10A RMS. However, rated current is different from the nominal current which is determined by minimum current that meets the claimed accuracy standard, such as IEC62053-22 and IEC60687.
פורסם עבור:שניידר אלקטריק ישראל