Below is an example using the "ServerisOnline" function. If you prefer to see 'Online' or 'Offline' instead of 1 for online and 0 for offline, you can add 2 more string parameters and do some comparisons to display a message showing I/O Status.
You can copy the cicode below to your project and rename the IOservers to your IOserver names.
FUNCTIONIOServerConnected()
INT itemp1,itemp2;
//Checks if the standby IOServer is online in this example the standby IO server is "IOServerS" if itemp = 1 then it is online
itemp1 =ServerIsOnline("IOServerS","Cluster1");
Message("Standby IO",itemp1,0);
//Checks if the Primary IOServer is online in this example the primary IO server is "IOServerP" if itemp = 1 then it is online
itemp2 =ServerIsOnline("IOServerP","Cluster1");
Message("Primary IO",itemp2,0);
END
Legacy KB System (APS) Data: RESL211553 V1.0, Originally authored by RaDe on 05/24/2013, Last Edited by RaDe on 05/24/2013
Related ranges: PowerSCADA Expert 7.3, PowerSCADA Expert 7.2, PowerLogic SCADA 7.1
פורסם עבור:שניידר אלקטריק ישראל