KB Article
Summary
This article describes how to configure a Meter display using ION Setup 2.0 to show any ION Handle.
Keywords
ION Setup V2.0, handle, display
Resolution
- 1. Find the ION handle for the register that is to be displayed in the Meter. See KB article 10685 for more information.
2. Right-click applicable meter, select Properties, select Show Advanced ION Setup.
3. Select display module to be changed, or add a new display module (if necessary).
4. Enter handle into Parameter field.
5. Hit Search, OK, Send
פורסם עבור:שניידר אלקטריק ישראל