המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
        
איך נוכל לעזור לך היום?
Momentum 171CCC98030 Ethernet processor maximum number of concurrent socket connections.

Goals and Symptoms

What is the maximum number of concurrent socket connections?

Causes and Fixes:

A maximum of 96 devices may be communicating with the processor adapter via the Ethernet at any one time.
This 96-device limit consists of:

  • · up to 2 programming panels (one must be in monitor mode)
    · up to 14 general purpose Modbus server paths (ex. Incoming SCADA requests) (Server)
    · up to 16 MSTR elements which support Modbus read, write, or read/write commands (Client)
    · up to 64 cyclic configured data slave paths (I/O Scanner) (Client)