המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
        
איך נוכל לעזור לך היום?
SMTP server returned error “Illegal address syntax from unknown in MAIL command:” when emailing the historical logs from an EGX300
Issue
The SMTP server returned the following error:
 
Nov 26 09:16:03 ip-10-10-20-165 postfix/smtpd[23309]: warning: Illegal address syntax from unknown[192.168.0.64] in MAIL command: test@Schneider-electric.com
 
Also, the diagnostic page of the EGX300 shows a "connection error" under the SMTP portion.

Product Line
EGX300 

Environment

EGX300 built in webpage configuration 

Cause
The From Address: and To Address: are not in a format that the SMTP server recognizes. 
  SMTP server returned error “Illegal address syntax from unknown in MAIL command:” when emailing the historical logs from an EGX300
 

 
 
Resolution
Add the signs "<" and ">" to the From Address: and To Address: fields. 

SMTP server returned error “Illegal address syntax from unknown in MAIL command:” when emailing the historical logs from an EGX300
Now, verify proper email operation.