Issue
What are the Modbus port designations on a Unity Momentum M1 and M1E
Product Line
Unity Momentum, Unity Pro
Resolution
When using a Unity Momentum M1, the Modbus ports are designated as MB port 0 and MB port 1.
When using a Unity Momentum M1E, the Modbus port is designated as MB port 0.
פורסם עבור: שניידר אלקטריק ישראל