{}

המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
Event Notification Module custom message field [ACTIVETIME] does not return the correct year.
Event Notification Module custom message field [ACTIVETIME] does not return the correct year.

In the Delivery Relays setup of ENM the user is able to setup custom messages using OPC Fields.

IF you use the field [ACTIVETIME] there is an issue where it adds 1600 to the year.

As a work around, during setup make sure you denote the full format you want the Active Time displayed as.

Example:
[ACTIVETIME: MM/dd/yyyy]

MM for month
dd for day
yyyy for year

Make sure you get the capitalization correct.

Using this full format will get the correct year.

שניידר אלקטריק ישראל