Issue:
Multiloader not recognizing SD card.
Product Line:
Altivar 61, Altivar 312, Altivar 31, Altivar 32, Altivar 71, Altivar 12, Altivar 212
Environment:
All
Cause:
Need to save a file on SD card and transfer to PC.
Resolution:
The Multi-Loader supports only FAT16 or FAT32 as file system. If SD card is formatted as NTFS, it will not work on it.
Solution is to format again the SD card to FAT32.
פורסם עבור:שניידר אלקטריק ישראל