Issue: Unable to configure GOOSE inputs for Vamp protection relays
Resolution: To be able to configure the GOOSE inputs for a VAMP relay you must select the Edition 2 Extensions check box when building the ICD file for the VAMP protection relay from VAMPset. This is what enables the GOOSE input configuration for the ICD file within VAMP SCD Editor.
Resolution: To be able to configure the GOOSE inputs for a VAMP relay you must select the Edition 2 Extensions check box when building the ICD file for the VAMP protection relay from VAMPset. This is what enables the GOOSE input configuration for the ICD file within VAMP SCD Editor.