Issue:
SoMove O-scope trigger function
Product Line:
ATV12, ATV312, ATV32, ATV61, ATV71, ATS22, ATS48, ATV320, ATV340, ATV630, ATV930
Envoronment:
All Serial numbers
Cause:
None
Resolution:
Logic inputs can be used as a scope trigger in SoMove V2.6.
SoMove O-scope trigger function
Product Line:
ATV12, ATV312, ATV32, ATV61, ATV71, ATS22, ATS48, ATV320, ATV340, ATV630, ATV930
Envoronment:
All Serial numbers
Cause:
None
Resolution:
Logic inputs can be used as a scope trigger in SoMove V2.6.
פורסם עבור:שניידר אלקטריק ישראל