{}

המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
PowerNet SNMP MIB will not compile or load due to error with Integer32 and/or Unsigned32

Issue

Some users have reported an error while trying to load and/or compile the APC PowerNet MIB recently. The error may be similar to: "Problem found when compiling the MIB: ERROR: Cannot find symbol Integer32, Source: Powernet412.mib, Row: 6761, Col: 11 SYNTAX Integer32" and also apply to Unsigned32 values.


Product Line
  • APC PowerNet SNMP MIB


Cause

It appears certain compilers and SNMP NMS systems are having problems finding the definition for Integer32 and Unsigned32 values which are defined under the IMPORTS section of the MIB. APC's MIB has not changed this recently.


Resolution

This will be addressed in a future MIB release. A workaround today is to manually edit the MIB in a text editor to contain the correct definition and references, as needed.

The MIB IMPORTS section looks like this today:
IMPORTS
enterprises, IpAddress, Gauge, TimeTicks            FROM RFC1155-SMI
DisplayString                                                          FROM RFC1213-MIB
OBJECT-TYPE                                                      FROM RFC-1212
TRAP-TYPE                                                           FROM RFC-1215;
-- IMPORTS End



The MIB IMPORTS section can be edited as shown below:
IMPORTS
enterprises, IpAddress, Gauge, TimeTicks             FROM RFC1155-SMI
DisplayString                                                           FROM RFC1213-MIB
OBJECT-TYPE                                                        FROM RFC-1212
Unsigned32, Integer32                                            FROM SNMPv2-SMI
TRAP-TYPE                                                              FROM RFC-1215;
-- IMPORTS End


With this adjustment, then the MIB should load and compile properly.

שניידר אלקטריק ישראל