המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
        
איך נוכל לעזור לך היום?
Video: Where can I find the serial number on ATV61 and ATV71 drives?
Issue:
ATV71 Where can I find the drive serial number if the drive is not powered up?

Product Line:
Altivar 61/71

Environment:
All

Cause:
Requested in documentation

Resolution:
Look for the product label mounted externally on the side of the drive. The serial number is under the barcode. The number typically begins with 88 , 8B , EL, 6W.
If the drive is powered, use the LCD graphic keypad to navigate to the Drive Menu, 1.11 IDENTIFICATION.  The serial number is just beneath the MC software Version.


Bar code image
                      Example