המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
        
איך נוכל לעזור לך היום?
What is the input voltage tolerance on the ATV61 and ATV71 series drives?
Issue:
Input voltage tolerance on the ATV61 and ATV71

Product Line:
Altivar 61 & 71

Environment:
All models, All serial numbers.

Cause:
Input voltage tolerance range needed.

Resolution:
For single phase input, part # ATV61H075M3 through ATV61HU75M3:  200 -15% to 240 +10%
For three phase input, part # ATV61H***M3 and ATV61H***M3X:  200 -15% to 240 +10%
For three phase input, part # ATV61****N4 and ATV61W***N4C:  380 -15% to 480 +10%
For three phase input, part # ATV61H***Y:  500 -15% to 690 +10%


For single phase input, part # ATV71H075M3 through ATV71HU75M3:  200 -15% to 240 +10%
For three phase input, part # ATV71H***M3 and ATV71H***M3X:  200 -15% to 240 +10%
For three phase input, part # ATV71****N4 and ATV71W***N4C:  380 -15% to 480 +10%
For three phase input, part # ATV71H***Y:  500 -15% to 690 +10%