המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
        
איך נוכל לעזור לך היום?
What are the limitations of the Modbus TCP IO Scanner of a TM251MESE?

The limitation of the Modbus TCP IO Scanner of a TM251MESE are:
- maximum 64 channels divided between maximum 64 slaves.
Each channel has the following limitations:
- for Read/Write Holding Registers the maximum length is 125 read words  and 121 write words
- for Read Holding Registers the maximum length is 125 words
- for Write Multiple Registers the maximum length is 123 words

 

If this FAQ did not solve your issue, you can chat with us at  chat with us  or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)