Each thermometer has a diagram presenting the alarm and trip circuits connected to the terminal in an idle stage for Oil Distribution Transformers.Closed circuits open and opened circuits close after exceeding the temperature threshold. Way of interpretation is up to the user. Please refer to the diagrams.