Yes. The only thing to take notice of is that the Modbus Plus tap assembly part# 990NAD23000 module sets termination by jumper settings whereas the ASMBKT-185 connector has a built-in termination and the ASMBKT-085 connector is non terminated for in-line connections.
פורסם עבור: שניידר אלקטריק ישראל