Yes, it is possible to change the labeling of the data in the disturbance recording. Unfortunately, you need to do it every time the disturbance recording is being viewed in SFT2826 or other tool. The automatic customization of the labeling is not possible because the labels are embedded in the Sepam itself.
פורסם עבור:שניידר אלקטריק ישראל