Issue:
ATV212 BacNet Communication
Product Line:
Altivar 212
Environment:
All serial numbers
Cause:
BacNet communication programming option
Resolution:
On the ATV212, the BacNet option is standard on the VFD. The BacNet is setup in drive programming and does not require a BacNet option card.
ATV212 BacNet Communication
Product Line:
Altivar 212
Environment:
All serial numbers
Cause:
BacNet communication programming option
Resolution:
On the ATV212, the BacNet option is standard on the VFD. The BacNet is setup in drive programming and does not require a BacNet option card.
פורסם עבור:שניידר אלקטריק ישראל