{}

המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
Which Modbus TCP/IP driver should we use in Vijeo Designer?
Issue:
It is unclear which Modbus TCP/IP driver to use in Vijeo Designer.

Product Line:
Vijeo Designer (all versions)

Resolution:
To select the correct driver, you must determine if the device you wish to connect to is a Modbus Client (requestor) or if the device is a Modbus Server (responder).

HMI (Client) ---> PLC or Device (Server):
If the device outside the HMI is the Modbus server, the best driver is to use the Modbus TCP/IP driver. This makes the HMI the Client and the device the "PLC". The HMI will read the device's Modbus registers like a regular PLC.

Device (Client) ---> HMI (Server):
If the device which is talking to the HMI is the Client, the best driver to use is the Modbus TCP Server driver of Vijeo Designer. This makes the HMI essentially act like a typical PLC and the client device outside of the HMI will read the HMI's own internal Modbus registers.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)