{}

המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
שאלות נפוצות
How to uninstall Ecoreach if the uninstall is unsuccessful while uninstalling from control panel>Program and Features>Uninstall or change a program?
The “EcoreachUninstaller” is useful when there is a problem with ecoreach uninstallation. Usually, the ecoreach uninstallation problems occur when the Ecoreach.msi is not found or deleted from the computer which has ecoreach already installed.
For running this program on windows 10 and windows 8 remember to right click on the EcoreachUninstaller executable and select “Run as Administrator” option.
Here are the steps to be followed to uninstall Ecoreach using the “EcoreachUninstaller”: -
  1. Copy the “EcoreachUninstaller.exe” and “MicrosoftProgram_Install_and_Uninstall.meta” at the same location. (Zipped folder containing both the files are attached.)
  2. Execute the “EcoreachUninstaller.exe” by clicking the “EcoreachUninstaller.exe”.
  3. The command prompt will start, follow the instructions on the command prompt to uninstall ecoreach. (Computer may restart.)
  4. On the command prompt, the status of uninstallation will be displayed. (Uninstallation Successful!!!) or (Uninstallation unsuccessful!!!).
  5. Once the uninstallation is successful, ecoreach can be reinstalled.
Confirm the successful uninstallation from Control Panel => “Program and Features/Uninstall or change a program”.

שניידר אלקטריק ישראל

קבצים מצורפים
Ecoreach_Uninstaller.7z [240.02 KB]