המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
        
איך נוכל לעזור לך היום?
Video: How to reset an Air Filter Run Hours violation alarm on a Uniflair Unit
Issue:
This video shows how to reset an Air Filter Run Hours violation alarm on a Uniflair Unit.
 
Product line:
All Unfair Units with Push-Button Display, All Chilled Water Uniflairs.
 
Environment:
All Serial Number with Push-Button Units.
 
Cause:
Repair, Install, Maintenance.
 
Resolution
 
To clear Air filters run  hour violations from a Uniflair push button display.
 
Press <> PRG.
 
Settings Menu <> ENTER.
 
Code <> 00000 ENTER.
 
Hour-Meter Settings <> ENTER.
 
ENTER down to reset hit ENTER change display to OK and then ENTER Again.
 
Alarm has been cleared. Review the following video for a demonstration of this procedure.