Issue
After modifying a PowerSCADA Expert project, the user would like to know which steps must be taken to make them active in Runtime.
Product Line
PowerSCADA Operation 8.2
PowerSCADA Operation 9.0
Environment
PowerSCADA Expert Runtime
Resolution
Note: The above table is intended for PowerSCADA Expert 8.2. You may use the table as a reference for previous versions, however there has been no testing to validate these recommendations.
After modifying a PowerSCADA Expert project, the user would like to know which steps must be taken to make them active in Runtime.
Product Line
PowerSCADA Operation 8.2
PowerSCADA Operation 9.0
Environment
PowerSCADA Expert Runtime
Resolution
Changes Being Made | Compile | Restart Client HMI | Reload Alarm Server | Reload Trend Server | Restart I/O Server | Stop and Start Schneider Electric Core Service Host |
Modify existing graphics pages including embedded Cicode | Yes | No | No | No | No | No |
Add completely new graphics page(s) | Yes | Yes | No | No | No | No |
Changes to PowerSCADA users (by using Cicode runtime CreateUser function) | No | No | No | No | No | No |
Changes to Active Directory group membership | No | No | No | No | No | No |
Changes to roles and Windows Active Directory group mapping | Yes | No | No | No | Yes | No |
Changes to users and/or roles (by using the PowerSCADA Studio) | Yes | No | No | No | Yes | No |
Changes to menu properties | Yes | No | No | No | No | No |
Changes to server-side Cicode | Yes | No | No | No | Yes | No |
Add/remove/modify alarm tags | Yes | No | Yes | No | Yes | Yes (if you need to update immediately) |
Add/remove/modify trend tags | Yes | No | No | Yes | No | Yes (if you need to update immediately) |
Add/remove/modify devices and/or variable tags | Yes | No | No | Yes | No | Yes (if you need to update immediately) |
Note: The above table is intended for PowerSCADA Expert 8.2. You may use the table as a reference for previous versions, however there has been no testing to validate these recommendations.
פורסם עבור:שניידר אלקטריק ישראל