שאלות נפוצות
Installation of LC1F800 turned 90 deg. from standard (vertical) position.
Side turning 90 deg. from standard position (main pole connection to the left and right) is possible for LC1F800.
However, the position for aux. contacts on LC1F800 has to be up - see Attachment1.
The installation with position for aux. contacts on LC1F800 down is not allowed.
However, the position for aux. contacts on LC1F800 has to be up - see Attachment1.
The installation with position for aux. contacts on LC1F800 down is not allowed.
פורסם עבור:שניידר אלקטריק ישראל
קבצים מצורפים
גלה עוד
טווח:
גלה עוד
טווח: