Is it possible to do the firmware upgrade of Enerlin'X devices like the IFE, IFM using Ecoreach when there is no breaker connected to the IMU?Using Ecoreach 2.5 or later, users can perform a firmware upgrade of ULP devices without connecting the ULP network to an IMU.
פורסם עבור:שניידר אלקטריק ישראל