שאלות נפוצות
Video: Connecting the Unity DTM Browser to the BMENOC0301 module
Issue
Establishing a connection between the Unity Pro DTM Browser to the Modicon M580 BMENOC0301 Ethernet Module.
Product Line
M580 BMENOC0301
Environment
Control Expert DTM Browser
Resolution
Below is a video that shows how to setup the Unity DTM Browser to connect to the BMENOC0301 module.
Connectivity requires the selection of the correct Source IP Address (PC) that will be used by Unity to connect.
Establishing a connection between the Unity Pro DTM Browser to the Modicon M580 BMENOC0301 Ethernet Module.
Product Line
M580 BMENOC0301
Environment
Control Expert DTM Browser
Resolution
Below is a video that shows how to setup the Unity DTM Browser to connect to the BMENOC0301 module.
Connectivity requires the selection of the correct Source IP Address (PC) that will be used by Unity to connect.
פורסם עבור:שניידר אלקטריק ישראל
גלה עוד
טווח:
גלה עוד
טווח: