המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
        
איך נוכל לעזור לך היום?
Video: How to change the size of the System Keypad in Vijeo Designer
Issue:
Adjusting the system keypad size in Vijeo Designer.

Product Line:
Vijeo Designer,  all serial numbers, all localizations, and all revisions.

Environment:
Vijeo Designer

Resolution:



To change the system keypad size in Vijeo Designer, you have 3 options:

1) Standard Keyboard
2) Compact (Multi-pages)
3) Alphabetical Order

To change the property, please go to the Target Property Inspector and change the System Keypad property.