What is the input disconnector on ATV650C25N4F? Is there an input load-break switch (can disconnect nominal currents ) or disconnector?It is INS630 (3-pole 630A switch disconnector) that is used as input switch-disconnector. It can be switched off under nominal current.
פורסם עבור:שניידר אלקטריק ישראל