Issue:
Cannot find a DNP3 Protocol in Vijeo Designer. Is it supported by the Magelis HMIs?
Product Line:
Vijeo Designer (all versions)
Resolution:
The Vijeo Designer Runtime does not support the DNP3 Protocol. Considering using a M340 PLC to communicate over DNP3 and then have the Vijeo Designer Runtime communicate to the M340 PLC over Modbus TCP/IP.
Cannot find a DNP3 Protocol in Vijeo Designer. Is it supported by the Magelis HMIs?
Product Line:
Vijeo Designer (all versions)
Resolution:
The Vijeo Designer Runtime does not support the DNP3 Protocol. Considering using a M340 PLC to communicate over DNP3 and then have the Vijeo Designer Runtime communicate to the M340 PLC over Modbus TCP/IP.
פורסם עבור:שניידר אלקטריק ישראל