Issue:
What is the Maximum number of BMXNOR0200 module which can be installed with a Modicon M580 CPU local rack?
Product Line:
BMXNOR0200H
Environment:
All
Resolution:
The maximum number of BMXNOR0200 which can be installed within a local rack containing M580 CPU is 6.
It also depends on the model of M580 CPU is being used.
1. BMEP58 6040 can accommodate 6 BMXNOR0200 modules.
2. BMEP58 5040 can accommodate 4 BMXNOR0200 modules.
3. BMEP58 4040 can accommodate 4 BMXNOR0200 modules.
4. BMEP58 4020 can accommodate 4 BMXNOR0200 modules.
5. BMEP58 3040 can accommodate 3 BMXNOR0200 modules.
6. BMEP58 3020 can accommodate 3 BMXNOR0200 modules.
7. BMEP58 2040 can accommodate 2 BMXNOR0200 modules.
8. BMEP58 2020 can accommodate 2 BMXNOR0200 modules.
9. BMEP58 1020 can accommodate 2 BMXNOR0200 modules.
פורסם עבור:שניידר אלקטריק ישראל