המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
        
איך נוכל לעזור לך היום?
How is Unity digitally signed.
Issue
How is Unity digitally signed.

Product Line
Unity

Environment  
Windows 10


Resolution
During startup, Unity performs a check on the '.dll' files that is uses.  When it sees that the security checksum does not correspond to the calculated checksum
that was created during the installation of the software or the recalculated checksum created after installing a hotfix, it displays a warning message
indicating that the '.dll' is faulty.