Does RealStream Lift Station allow submersible pump sensors to be connected to it?
The RealStream Lift Station allows the submersible pump sensor relays like temperature and seal failure to be fed directly into the controller, which will automatically stop the pump if configured.