המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can I add a delay in a script action in Vijeo Designer V6.2
There is no delay script method in Vijeo Designer.  It is not recommended to create a loop as a workaround since it can make the HMI very slow and effect the communication or even lock up the HMI
If you are calling the script from a switch , you can split your script in half and add a delay operation.  This delay operation is only available from a switch operation.  So if the script is called from a local or global action it cannot be done.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

שניידר אלקטריק ישראל

קבצים מצורפים
VJDScript_delay.jpg [178.66 KB]