Issue:
INF2 or internal error 2 on the ATV630 and ATV930 Process drives.
Product Line:
ATV630 and ATV930 Process drives
Environment:
All
Cause:
The Power board was exchanged by a spare part, and is not configurable to the correct power rating.
Resolution:
Unknown or Incompatible Power Board
Principle
Probable causes:
• The Power board was exchanged by a spare part, and is not configurable to the correct power rating.
Remedies
• Switch OFF/ON the inverter.
• Check the reference number of the power board.
• connect to the SoMove service section and use the "drive type recovery function" to set a valid configuration of the power board.
• Replace the control block
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
פורסם עבור:שניידר אלקטריק ישראל